NFC PN532 radio parameters in ISO/IEC 14443 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC PN532 radio parameters in ISO/IEC 14443 mode

638 Views
rcbtactiq
Contributor I

Can NXP please provide the following information for the PN532 device while operating with IEC 14443 compliant NFC tags?

  • ITU emission designator(s)
  • Channel bandwidth
  • Output power
  • Nominal duty cycle of Tx and class
  • Maximum duty cycle of Tx

 

I was unable to find this in the datasheet / user manual

Kind regards

Reuben

Labels (1)
0 Kudos
1 Reply

419 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Reuben,

Actually these parameters depends on your application, and controlled by the up layer application code, please kindly refer to Types of radio emissions - Wikipedia  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos