AnsweredAssumed Answered

i.mx6dl LVDS 1366x768 OpenGL Support

Question asked by Hichem Ben Fekih on Dec 7, 2016
Latest reply on Jan 31, 2017 by Wolfgang Netbal

Hello,

 

I hope, this time I will get some support.

the following was my first post. since I did not received any help, I thought maybe I post the problem again .

I.MX6DL + LVDS Display 1366x782 + OpenGL ES + QT 

 

we have developed a custom Board based on i.mx6dl. the board is connected via LVDS to Display.

we have successfully tested the board with 1280x800 and 1920x1080 Displays.

 

the issue with the 1366x768 Display is that, I can not run the GPU-examples provided by NXP/Freescale

if I change the Display resolution to 1364x768, then the GPU-exmaples can be started, but a white bar is shown (on the left or on the right side) (maybe 8 pixel wide).

 

we are using a custom kernel build 3.14.52_1.0.0_ga-wandboard and Galcore Kernel module version 5.0.11.41671

(I had the same problem with our reference board "wandboard")

 

it will be very nice if I get some comments.

Thank you in advance. 

Hichem,

CANNON-Automata

Outcomes