Question of MCP577C MCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question of MCP577C MCAN

787 Views
Luke_Chun
NXP Employee
NXP Employee

Hello Team

 

Could you check the question of MCP577C MCAN?

 

When I checked the 41.3.3 Data Bit Timing and Prescaler Register (M_CAN_DBTP) on 5777C RM Rev.7, I found the below mention.


The CAN bit time may be programed in the range of 4 to 49 time quanta.

 

As my known, thq above mention's means that 4~49 means the sum of [DTSEG1 + DTSEG2 + 3]…


However the minimum value of DTSEG1 and DTSEG2 is “0”…..

So the programed in the range is possible to 3 to 49…([0 + 0 + 3] ~ [ 0x1f + 0xf + 3]) if I use the below register information.

 

Could you check this question?

 

170841_170841.pngpastedImage_1.png

 

Thank you.

Labels (1)
2 Replies

576 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Luke,

I assume one of the DTSEG1 or DTSEG2 could have valid value from 1, but let me check this with Apps.

BR, Petr

576 Views
Luke_Chun
NXP Employee
NXP Employee

Hello PetrS

Could you check my question?

As my checking on MPC5777C RM Rev.7, it is showing min value = 0 both DTSEG1 and DTSEG2. 

Thank you.

0 Kudos