AnsweredAssumed Answered

We are using LS1043A, in that we are using both EC1 and EC2.

Question asked by Logesh S on Dec 2, 2016
Latest reply on Dec 4, 2016 by Logesh S

Both EC1 and EC2 are connected as RGMII. We have connected EC1 to one PHY and EC2 to Switch. Can we use either EMI1/EMI2 alone (single management Interface) for both EC1 and EC2?

Suppose if we use both Management interface EMI1 and EMI2, shall we connect any of the management interface EMI to either of EC1 or EC2? is there any restriction that EC1 should be connected with EMI1 & EC2 with EMI2? 

Outcomes