Does i.MX6 SoloX has an GPU SDK for Cortex-M4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 SoloX has an GPU SDK for Cortex-M4?

Jump to solution
574 Views
m_c
Senior Contributor I

Customer would like to implement cluster function by i.MX6 SoloX Cortex-M4. Does i.MX6 SoloX has an GPU SDK for Cortex-M4?

Below is from i.MX6 SoloX reference manual.

33.5 Usage Mode
The GPU should be programmed through the Freescale provided driver. Freescale does
not provide support for software that directly programs the GPU registers. APIs for
programming the GPU through the software driver are described in separate driver
documentation.

Labels (2)
0 Kudos
1 Solution
390 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

nxp bsps have linux gpu drivers operating using linux apis.

Cortex-M4 runs rtos and such drivers are not provided.

Best regards
igor
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
391 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

nxp bsps have linux gpu drivers operating using linux apis.

Cortex-M4 runs rtos and such drivers are not provided.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos