Memory Dump for MC56F84550

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory Dump for MC56F84550

1,352 Views
vasilkostadinow
Contributor I

Dear PGO, how can I read the flash content of that DSC? I saw that it's in list of MC56F programmer, but not in Memory dump.

Labels (1)
0 Kudos
1 Reply

952 Views
pgo
Senior Contributor V

Hi Vasil,

The support for MC56F device in USBDM is very limited.

The device family is very different from the other supported families and it has a lot of "special case" code that can't be shared with the other families.  The effort to add new devices is quite high.

For both of these reasons I have done little recently to support these devices.

I will have a look at how difficult it would be to add basic MC56F support to the memory dump program but it is unlikely to be any time soon,

Sorry.

bye

0 Kudos