what is the process geometry (nano meter specs) for MC9S12 CPUs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the process geometry (nano meter specs) for MC9S12 CPUs?

507 Views
tommctaggart
Contributor I

What is the process geometry size for the MC9S12 CPU, please?

Labels (1)
0 Kudos
1 Reply

393 Views
iggi
NXP Employee
NXP Employee

Hi Tom,

The most of the MC9S12 device families which are active and in production are based on 180nm process technology such as S12XE, S12G and MagniV devices based on S12Z core such as S12ZVM, S12ZVL, S12ZVC etc.

Some other families are based on 250nm process technology such as S12A/B/C/D/E, S12P, S12XD and few more.

Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos