Greetings,
I was curious if you have a specific battery from any manufacturer that you can share with me that can be used in Sabre SD Board. This board has a BK414 type retainer however I cant find many batteries suitable. In our custom board I used the exact same retianer so now am struggling with finding a suitable cell.
Do sabre boards come with one installed? If so which one?
Regards,
Mete
Please refer to the attached document. It specifies the suitable battery part numbers as ML414, MS412FE, MS414GE.
Q. Do sabre boards come with one installed?
A. No.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
Thanks for the part numbers. Cant see the attachment though?
Mete