AnsweredAssumed Answered

Can anyone provide the procedure to enable hardware acceleration in Yocto dizzy for qt5?

Question asked by Ambika . on Nov 25, 2016
Latest reply on Nov 27, 2016 by igorpadykov

Hi,

 

I'm working on imx6q processor.

 

We are running QT application which has the displaying image in some pattern continuously, there its frame rate is around 10 fps and it uses 100% of CPU.

Where as when I run the same pattern using OpenGL frame rate is 56 to 60 fps and CPU usage is not more than 20%.

 

Seems like OpenGL is using hardware acceleration and QT is not using. If so.. Can anybody let know to enable hardware acceleration in QT of Yocto dizzy release??

 

I appreciate your help  

Thanks in advance.

 

Regards,

Ambika

Outcomes