AnsweredAssumed Answered

Regarding USB Usage in LPC4357

Question asked by sudheer kumar doredla on Nov 24, 2016
Latest reply on Dec 30, 2016 by soledad

Dear All,

 

I want to use the USB in LPC4357 , for the Application of sending the large amount of data to modem , but modem class, protocol and interface are Vendor specific. so Shall I use this one as CDC class device.

 

 

if we use microcontroller as Host, is it possible to receive the data with out host request. (Any interrupt data supported by microcontroller it self). (ex: If we get any in coming call to chipset, that we will directly intimate to mcu or Host need to pool every time for any data).

 

Help the above questions.

 

Provide the USB Host drivers for LPC4357.

Outcomes