Hello,
We are designing a PCB with IMX6UL processor(Part No: MCIMX6G2DVM05AA).
According to TAMPER_PIN_DISABLE[1:0] ,the pins can either be enabled for tamper detection or used as GPIO.
(Please find the following configuration as on Pg214 of IMX6UL reference manual.)
Also page 131 of IMX6UL datasheet specifies that 1M to be added in the following conditions.
1.When the tamper pins are configured as GPIOs
2.When the pins are enabled for tamper detection.
Q1: Does the above reference means that 1M resistor be added to the SNVS_TAMPER pins, on all the above cases.
Also can you please clarify the handling of SNVS_TAMPER pins in the design, for the following conditions.
Q2.The SNVS tamper pins are not used either as GPIOs or for tamper detection function.
Does all the 10 pins (SNVS_TAMPER[0:9]) require 1M resistor to GND(or pulled up to SNVS).
Can the pins be left floating ?
Q3.Only certain tamper pins are configured as GPIOs(as specified by the bits in TAMPER_PIN_DISABLE[1:0]) in SNVS_TAMPER[0:9].Can 1M pull down/pull up resistors be added only for them.
Thanks in anticipation.
Solved! Go to Solution.
Hello,
The case, when the SNVS_TAMPER pins are configured as tampers and tamper functions
are used, there is no need for the 1M resistor : external scheme should provide expected
voltage level for tamper event.
If power consumption is not the problem for Your system it is possible to configure
the pins as GPIO input and use internal resistors for pulling or keepers.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------
Hello,
The case, when the SNVS_TAMPER pins are configured as tampers and tamper functions
are used, there is no need for the 1M resistor : external scheme should provide expected
voltage level for tamper event.
If power consumption is not the problem for Your system it is possible to configure
the pins as GPIO input and use internal resistors for pulling or keepers.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------