Hello,
i.mx6soloX used as EP, X86 used as RC, refrence clk input i.MX6soloX CCM_CLK1_N pin, I found i.mx6solox can't start.
Could you please help advise i.mx6solox if support outside clk input(I know i.mx6Q is ok)? if it's OK, Clk input ccm_clk1_p/n pin?, What need I configue in hardware and sorftware?
Thanks a lot.
Hello
from the design checklist :
"PCIe reference clock solution which provided by CLKx_N/P of i.MX6 chip can't pass PCIe Gen2 compliance test. Recommend using external PCIe 2.0/3.0 clock generator with 2 HCSL outputs solution. One clock channel connect
to i.MX6 as a reference input, another clock channel should connect to PCIe connector ..."
https://community.nxp.com/docs/DOC-329599
http://www.nxp.com/assets/documents/data/en/application-notes/AN5158.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------