imx6 OpenCV 3.0 @ 4..15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 OpenCV 3.0 @ 4..15

1,040 Views
erikraynolds
Contributor III

Dears,

I'd like to create a Yocot image build for imx-4.1.15-1.0.0_ga to include OpenCV 3.0. I see recipe opencv_3.0.bb how should I use/configure a build to have 3.0 instead of 2.4? 

Now compiling & build creates opencv lib out of 2.4 so I wan to have 3.0..  

Thank you.

Tags (1)
0 Kudos
1 Reply

412 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Erik,

please take a look to this post.

Yocto and OpenCV 3 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos