AnsweredAssumed Answered

DDR4 Compatibility with T1042

Question asked by Gokul Krishnan on Nov 23, 2016
Latest reply on Nov 23, 2016 by Serguei Podiatchev

Hi, 

I am planning on using a DDR4 memory chip along with the T1042 processor. From the datasheet i found that the chip only supports upto 1600 in data rate and has a max clock frequency of 800MHz.

While the DDR4 device requires a clock of 1333MHz. Could you clarify if this would work properly or Shoudl I choose some other configuration ?

 

Regards

Gokul

Outcomes