Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any way to connect the Magstripe Reader Head directly to the i.MX6?

566 Views
hrushinale
Contributor III

Hello All,

I want to interface the MSR with i.MX6 Dualite processor. As I search the sample I got the product with external USB interface but I want to interafce it directly to the processor .

Please Suggest me the solutions for the same.

Best Regards,

Hrushi

Tags (1)
0 Kudos
2 Replies

492 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

it depends on MSR model, if it has additional interfaces which could be

used for such purpose. So one can contact vendor or check MSR schematic.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

492 Views
hrushinale
Contributor III

Hello igorpadykov,

Thanks for your Reply.

can you suggest such MSR Models Part Number and Vendor Names which has such additional interfaces.

Best Regards,

Hrushi

0 Kudos