Hi,
I'd like to use KDS for KV4 or KV5 series. When they will be supported?
-Michael
Solved! Go to Solution.
Hello Michael,
Yes, the latest version of KDS v3.2 now have the KV4 option when create project on menu.
We can also development KV5 series chip on KDSv3.2, just need download KSDKv2.0 for the KV5x
chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0
Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,
just need select "Empty" on the Drivers:
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just noticed that KV4 is supported in th 3.2. release. All clear.
Hello Michael,
Yes, the latest version of KDS v3.2 now have the KV4 option when create project on menu.
We can also development KV5 series chip on KDSv3.2, just need download KSDKv2.0 for the KV5x
chips, refer to this DOC:Using Kinetis Design Studio v3.x with Kinetis SDK v2.0
Thus you can development on KDS. If you don't want to use the driver of KSDK, when you create project ,
just need select "Empty" on the Drivers:
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------