AnsweredAssumed Answered

About behavior of i.MX25 when Low was input into POWER_FAIL pin

Question asked by yuuki on Nov 22, 2016
Latest reply on Nov 22, 2016 by Yuri Muhin

Dear all,

 

We have a question about the function of the POWER_FAIL pin(T19 pin) of i.MX25.

 

The following is explained in the data sheet.

"An interrupt from PMIC, which should be connected to a low-battery detection circuit."

 

However, I was not able to find detailed explanation.

 

When T19 pin of i.MX25 is used as POWER_FAIL_INT function,
would you tell me the operation of i.MX25 when Low signal was input into this pin?
(When Low signal is input into this Pin, I want to know the behavior of i.MX25)

 

Best Regards,

Yuuki

Outcomes