P1010 USB documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 USB documentation

Jump to solution
447 Views
smirnovalexey
Contributor I

Hello.

In the P1010RM in USB section we have a list of external signals.

For example Table 17-1 have an USB_DRVVBUS I/O signal. At the same time in P1010EC we have no such signal.

The closest alternative i can find is GPIO_0/IRQ_4/DRVVBUS/MDVAL pin D23.

Am I correct?

It is very confusing because of USB prefix absence..

Thank you.

Labels (1)
0 Kudos
1 Solution
356 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.
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
357 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes, it is correct. Table 17-1 USB_DRVVBUS and DRVVBUS on pin D23 mean the same signal.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos