I am working in Panasonic and we have a NFC integrated Windows Tablet PC.
We are working for a project where customer require below things in NFC reader.
1. OS: Android/Windows
2. Encryption: AES (NFC module should have access to this)
3. SAM slot (Available in Device)
4. 3g / 4g / LTE SIM slot (Available in Device)
5. Communication: NFC with support for Felica ISO/IEC 18092 (212 kbps or 424 kbps Passive Communication Mode)
Pls suggest suitable NFC module for our device.
Device details are as follows.
Panasonic FZ-M1
NFC Module-NXP PR533