AnsweredAssumed Answered

I.MX6Q 从EMMC启动 随机无法启动的问题?

Question asked by Bruce Li on Nov 16, 2016
Latest reply on Nov 17, 2016 by Bruce Li

正常的板子启动 EMMC CLK 为374KHz, 然后切换到20M,50MHz。 无法启动的板子,EMMC CLK 起初为374KHz,后面切换到10M,16M,无法起来。(参看附件的波形)目前通过调试Core 供电电压1.33V和1.38V,没有变化。上电时序是VDD_HIGH_IN=VDD_SNVS_IN,3V3_HIGH_IN > 1.35V , 1.5V> 3.3V . 3V3上电后Delay 500ms POR_RST解复位。从现象上看,启动的内部ROM的状态机没有走到EMMC模式,这些都是BOOT_CFG配置的,如何解决这个问题,请大神帮忙看看,多谢?

Outcomes