Problems with SOT1174-1 Footprint information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with SOT1174-1 Footprint information

359 Views
janscholz
Contributor I

Hi,

I am trying to use a device in my design that is produced in SOT1174-1 package.

For that device I try to design a landpattern.

When I look for the Landpattern documentation, I end up in the footprint information, that is competly not understandable for me.

The measurements of the package are there with 2x2.3CU. CU is nowhere refered to. What does that mean? When I look for the Package outlines I see that the Package should be 2.0x1.7mm.

Many things are dimensioned with that CU parameter.

It would really be nice if I could get information about the Landpattern to give me the ability to create a Footprint that is matching my device later.

Regards,

Jan Scholz

1 Reply

268 Views
antalsoos
Contributor I

So what is the CU?

xxx.pngIt would be so difficult to include, explicitly, the marked dimensions?

Best Regards,

Antal

0 Kudos