iMX28 : Errata workaround implementation status for No 2858 in Linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 : Errata workaround implementation status for No 2858 in Linux BSP

Jump to solution
581 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with iMX28.

Sometimes the iMX28 hangs up, on connecting a USB device.

I checked the Errata list.
And I found the errata No 2858 "USB controller may access a wrong address for the dTD and then hangs"
I am using the Linux BSP ( L2.6.35_1.1.0_130130 ).

I hope to confirm the errata workaround implementation status .

[Question]
       Is this errata workaround implemented in Linux BSP ( L2.6.35_1.1.0_130130 ) ?

       Best Regards,
       Koichi Sakagami

Labels (2)
0 Kudos
1 Solution
459 Views
b36401
NXP Employee
NXP Employee

Unfortunately the errata presents in this BSP. Sorry for the inconvenience.
However you can try to build the OS using more recent BSP based on 3.10 kernel.
Our new kernels has additional dTD per each EP. It should avoid the issue.

Have a great day,
Victor
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
460 Views
b36401
NXP Employee
NXP Employee

Unfortunately the errata presents in this BSP. Sorry for the inconvenience.
However you can try to build the OS using more recent BSP based on 3.10 kernel.
Our new kernels has additional dTD per each EP. It should avoid the issue.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos