AnsweredAssumed Answered

DUART stops responding when stressed it by sending lots of data to LS1021A-TWR?

Question asked by Sk Hasanujjaman on Nov 14, 2016
Latest reply on Nov 15, 2016 by Pavel Chubakov

Hello,

 

I am developing the DUART driver for the board TWR-LS1021A-PB. DUART works fine as long as you don't stress it by sending lots of data to the target. In the situation when serial communication stops, if I reset the MBED controller (by plug in/plug out the USB cable), serial seems to work again. In my understanding the problem may be in the Windows driver (mbedWinSerial_16466.exe) or in the MBED firmware (k20dx128_if_mbed.bin). Please find below the details of my test environment.

 

Host PC: Windows x86

Serial Driver: mbedWinSerial_16466.exe

Serial Port Configuration: 115200-8-N-1

Host application: Send/receive data to/from the target board (TWR-LS1021A-PB). 

 

Target board: TWR-LS1021A-PB

UART controller: DUART1

Clock input to the UART controller : 150 MHz (Platform clock / 2, where Platform clock is 300 MHz)

Baud rate set : 115200 bps

 

During debugging, I have observed that the UART driver in the target board is still alive when the communication fails between the host and the target. That means if I reset the MBED controller the communication gets established again.

 

Has anyone faced this kind of issue? Is there any workaround?

 

Thanks.

Outcomes