I am looking for a downloadable eval copy of CodeWarrior for HCS12(X) Microcontrollers v5.2. I have a non-networked development machine that requires installation from a DVD,etc. Please advise, Thanks, TIm
Solved! Go to Solution.
Hi,
in addition, this is evaluation CWs (include CW5.2) download link:
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Tim
You can first download the installer in the PC which can connect to internet ,
then copy the installer package into U disk , then use it to install on the non-networked development machine .
Does this can help ?
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------