SPI1 configuration problem on MKM34Z256xxx7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI1 configuration problem on MKM34Z256xxx7

Jump to solution
785 Views
samdexter
Contributor II

It seems that SPI1 PTI0 ALT4 (SPI1_MISO) and PTI1 ALT4 (SPI1_MOSI) do not work on MKM34Z256xxx7.

The lines stay low during communication attempt, however, PTH6 ALT3 (SPI1_PCS0)) and PTH7 ALT3

(SPI1_CLK) function properly. Switching PTI pins to ALT5 make them to work as required, except for the

swapped functionality (MISO <-> MOSI).

Tested on a custom board and on MKM34Z7 tower board. Is it a bug on a silicon or I am doing something

wrong?

Can anybody confirm, please?

1 Solution
586 Views
MarMi
NXP Employee
NXP Employee

Helo Sam,

according to reference manual page 135:

PTI1 (This pin is true open drain pad. External pull-up resistor should be added.)

Kind regards,

Martin M.

View solution in original post

2 Replies
587 Views
MarMi
NXP Employee
NXP Employee

Helo Sam,

according to reference manual page 135:

PTI1 (This pin is true open drain pad. External pull-up resistor should be added.)

Kind regards,

Martin M.

586 Views
samdexter
Contributor II

Oh... That's embarrassing. How could I not pay attention to that note...

Will try it shortly. Thank you very much for pointing it out.

Regards,

Sam.

0 Kudos