MCIMX6D6AVT10AD thermal issue??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6D6AVT10AD thermal issue??

829 Views
bryantchou
Contributor I

Dear All:

 The "MCIMX6D6AVT10AD" is using on our project , but we meet  80 degree can't start up system and 100 degree shut down system issue.

  There are several question as blow:

  1. The "MCIMX6D6AVT10AD" is automotive grade that temperature range is -40 degree to 125 degree , but the thermal limit still set the 80 degree and 100 degree, why????

  cpu.jpg

  2. Does the thermal limit that  80 degree and 100 degree for all i.MX6 series???

  3. Can we adjust the thermal limit by ourself ???

   Thanks a lot for reply.

   Sincerely,

   Bryant Chou

0 Kudos
1 Reply

372 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bryant

this can be adjusted according to custom needs, please check example on

https://community.nxp.com/message/813309?commentID=813309#comment-813309

chapter Software Thermal Management Techniques

AN4579 http://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos