AnsweredAssumed Answered

MPC5775K boundary scan problem

Question asked by Zsolt Tako on Nov 9, 2016
Latest reply on Nov 10, 2016 by Lukas Zadrapa

I tried to start the boundary scan test on an SPC5775K micro (with mpc577xk_bga356 bsdl file), but the device doesn't communicate on the Test Access Port. In other bsdl files I see that there is a compliance enable pattern section, that specifies how to set the device into bsdl testing mode. In the actual bsdl file this section is empty. Could you please check if this information is missing from the bsdl file by mistake, or it is not needed? In the latter case how should I let the device know that it should receive commands on the Test Access Port?

 

This is the section from the bsdl file that I'm referring to:

-- Specifies the compliance enable patterns for the design. It lists a set of
-- design ports and the values that they should be set to, in order to enable
-- compliance to IEEE Std 1149.1

Outcomes