About PN5180's impedance,what is correct?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About PN5180's impedance,what is correct?

1,308 Views
wujiaqiang
Contributor I

The Fig 20 shows the driver current ITVDD versus the antenna impedance. The target impedance to get a maximum field strength and power transfer should be close to 20Ω.(PN5180 Antenna design guide.pdf)

QQ截图20151202170952.png

but the other part is 50Ohm,what is correct?

Tags (2)
0 Kudos
3 Replies

891 Views
ND2
Contributor III

Hi Wingros,

So the antenna tuning in this case should be done to match with 20Ohm or 50Ohm for maximum reading distance (not working on a battery).

Please suggest.

Neel.

0 Kudos

891 Views
ND2
Contributor III

@Wingros

Would be great to get a response here.

Neel.

0 Kudos

891 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Wu,

    20OHM impedance is between TX line & antenna;

    50OHM impedance is between signal line & GND.

Understand my explanation?

Best Regards,

Weidong