We are looking at running our VF610s at 500 MHz and are running into some issues. The custome have applied the 5))MHz patches that are ontop of u-boot 2013.07, provided by Timesys, against u-boot 2015.07 and see instability after 5 hours. Is there a patchset from NXP that also handle e6235 ( ANADIG: Unstable clock if PFD_FRAC divisor is 19)?
Is Timesys Uboot the latest to support 500Mhz or do we have more updated one?
Regards,
hy
Hello,
I am afraid we do not provide Linux BSP for Vybrid, assuming third party (Timesys) for it.
Regards,
Yuri.