I´m working with LPCXpresso v8.2.0 [Build 647] [2016-07-18] on LPC1769 & LPCOpen 2.10 (http://cache.nxp.com/files/microcontrollers/software/LPCWare/lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip) Powe Mode Use application (periph_pmu.zip) have a problem.
In debug mode when I press Resume (F8) the Sleep mode works OK, but the other three modes (Deep-Sleep, Power-down and Deep-Power-down) don´t work OK => debugging is stopped (see image or attached file).
Hi Hi Juan Manuel Cruz,
Thanks for your reply.
In the reference manual, it also recommend the user to re-configure the PLLs and clock dividers after the wake-up.
So it good to call the Chip_SetupXtalClocking() to re-configure the PLLs and clock dividers after the wake-up.
And I'll report the issue to the AE for checking.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------