AnsweredAssumed Answered

based on imx6 sabresd,customed board emmc double,DDR2 1G to DDR3 2G

Question asked by hong wu on Nov 8, 2016
Latest reply on Nov 13, 2016 by hong wu

i.MX Solutions

基于imx6q sabresd board, Android 4.3, jb4.3_1.0.0-ga source code.

公版内存是1G,eMMC容量为8G.

我们基于此定制的板子改为2G DDR3内存,16G eMMC.

使用MfgTool下载img到eMMC,可以下载成功(中途没有出错),而且下载完成后看串口信息kernel已经跑起来了。

但是下载完成后,断电,设置11010110从emmc启动,板子却起不来。

1. 是我配置的2G DDR3有问题吗,如果有问题下载的过程应该也无法继续吧。

2. eMMC容量增加一倍后需要配置eMMC吗,还是MfgTool会自动识别大小并进行分区。

 

请NXP相关工程师详细回复一下我应该如何正确配置。

 

附上下载时的串口信息:
CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Temperature: 29 C, calibration data 0x59e4eb7d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock : 66000000Hz

ipg per clock : 66000000Hz

uart clock : 80000000Hz

cspi clock : 60000000Hz

ahb clock : 132000000Hz

axi clock : 264000000Hz

emi_slow clock: 29333333Hz

ddr clock : 528000000Hz

usdhc1 clock : 198000000Hz

usdhc2 clock : 198000000Hz

usdhc3 clock : 198000000Hz

usdhc4 clock : 198000000Hz

nfc clock : 24000000Hz

Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]

Boot Device: SPI NOR

I2C: ready

DRAM: 1 GB

MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Using default environment


In: serial

Out: serial

Err: serial

Net: got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot: 0

## Booting kernel from Legacy Image at 10800000 ...

Image Name: Linux-3.0.35-2204-g931218f

Image Type: ARM Linux Kernel Image (uncompressed)

Data Size: 3151024 Bytes = 3 MB

Load Address: 10008000

Entry Point: 10008000

Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 10c00000 ...

Image Name: uboot initramfs rootfs

Image Type: ARM Linux RAMDisk Image (gzip compressed)

Data Size: 4545227 Bytes = 4.3 MB

Load Address: 00000000

Entry Point: 00000000

Verifying Checksum ... OK

Loading Kernel Image ... OK

OK


Starting kernel ...


Uncompressing Linux... done, booting the kernel.
Linux version 3.0.35-2204-g931218f (b21710@bluejay) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Mon Nov 19 13:56:38 CST 2012
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @8c008000 s5184 r8192 d15296 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 1028736k/1028736k available, 19840k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xf4600000 - 0xffe00000 ( 184 MB)
vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x80039000 ( 196 kB)
.text : 0x80039000 - 0x805a789c (5563 kB)
.data : 0x805a8000 - 0x805f15c0 ( 294 kB)
.bss : 0x805f15e4 - 0x8061c1b4 ( 171 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:496
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
IMX usb wakeup probe
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: SPKVDD: 4200 mV
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1375 mV
print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1375 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2500 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
max17135 2-0048: PMIC MAX17135 for eInk display
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode: dummy_timer is not functional.
dummy_timer is not functional.
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 1
Could not switch to high resolution mode on CPU 2
Could not switch to high resolution mode on CPU 3
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 0
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 4436K
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is disabled for i.MX6
cpaddr = c0880000 suspend_iram_base=c0918000
PM driver module loaded
i.MXC CPU frequency driver
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 2017
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.3: ipu1-di1 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
m25p80 spi0.0: unrecognized JEDEC id ffffff
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
add wake up source irq 75
g_file_storage gadget: controller 'fsl-usb2-udc' not recognized
check_parameters:UTP settings are in place now, overriding defaults
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
fsl-usb2-udc: bind to driver g_file_storage
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12
imx_3stack asoc driver
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
g_file_storage gadget: high speed config #1
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
Freeing init memory: 196K
Starting UTP
ln: /etc/mtab: File exists
disable turn off display
Starting the hotplug events dispatcher udevd
udevd (1995): /proc/1995/oom_adj is deprecated, please use /proc/1995/oom_score_adj instead.
Synthesizing initial hotplug events
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 SEM16G 14.8 GiB
mmcblk0boot0: mmc0:0001 SEM16G partition 1 1.00 MiB
mmcblk0boot1: mmc0:0001 SEM16G partition 2 1.00 MiB
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk0boot1: unknown partition table
mmcblk0boot0: unknown partition table
uuc 0.4 [built Nov 19 2012 01:38:37]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16"
16+0 records in
16+0 records out
8192 bytes (8.0KB) copied, 0.154811 seconds, 51.7KB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config'
UTP: executing "echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config"
UTP: sending Success to kernel for command $ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2 skip=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2 skip=2"
881+1 records in
881+1 records out
451212 bytes (440.6KB) copied, 0.255428 seconds, 1.7MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2 skip=2.
utp_poll: pass returned.
UTP: received command '$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config'
UTP: executing "echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config"
UTP: sending Success to kernel for command $ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard-android.sh /dev/mmcblk0'
UTP: executing "sh mksdcard-android.sh /dev/mmcblk0"
BOOT : 16MB
RECOVERY: 8MB
SYSTEM : 512MB
CACHE : 256MB
DATA : 2048MB
VENDER : 8MB
MISC : 8MB
VF mmcblk0: unknown partition table
AT : 12280MB
1+0 records in
1+0 records out
1024 bytes (1.0KB) copied, 0.001404 seconds, 712.3KB/s
Checking that no-one is using this disk right now ...
OK

Disk /dev/mmcblk0: 486016 cylinders, 4 heads, 16 sectors/track

sfdisk: ERROR: sector 0 does not have an msdos signature
/dev/mmcblk0: unrecognized partition table type
Old situation:
No partitions found
New situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 0+ 15 16- 16383+ 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 2895 2872 2940928 5 Extended
/dev/mmcblk0p4 2896 15175 12280 12574720 b W95 FAT32
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 791 256- 262143+ 83 Linux
/dev/mmcblk0p7 792+ 2839 2048- 2097151+ 83 Linux
/dev/mmcblk0p8 2840+ 2847 8- 8191+ 83 Linux
/dev/mmcblk0p9 2848+ 2855 8- 8191+ 83 Linux
Warning: no primary partition is marked bootable (active)
This does not matter for LILO, but the DOS MBR will not boot this disk.
Successfully wrote the new partition table

Re-reading the partition table ...
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
Checking that no-one is using this disk right now ...
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
OK

Disk /dev/mmcblk0: 486016 cylinders, 4 heads, 16 sectors/track
Old situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 0+ 15 16- 16383+ 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 2895 2872 2940928 5 Extended
/dev/mmcblk0p4 2896 15175 12280 12574720 b W95 FAT32
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 791 256- 262143+ 83 Linux
/dev/mmcblk0p7 792+ 2839 2048- 2097151+ 83 Linux
/dev/mmcblk0p8 2840+ 2847 8- 8191+ 83 Linux
/dev/mmcblk0p9 2848+ 2855 8- 8191+ 83 Linux
New situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 8 15 8 8192 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 2895 2872 2940928 5 Extended
/dev/mmcblk0p4 2896 15175 12280 12574720 b W95 FAT32
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 791 256- 262143+ 83 Linux
/dev/mmcblk0p7 792+ 2839 2048- 2097151+ 83 Linux
/dev/mmcblk0p8 2840+ 2847 8- 8191+ 83 Linux
/dev/mmcblk0p9 2848+ 2855 8- 8191+ 83 Linux
Warning: no primary partition is marked bootable (active)
This does not matter for LILO, but the DOS MBR will not boot this disk.
Successfully wrote the new partition table

Re-reading the partition table ...
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
UTP: sending Success to kernel for command $ sh mksdcard-android.sh /dev/mmcblk0.
utp_poll: pass returned.
UTP: received command '$ ls -l /dev/mmc* '
UTP: executing "ls -l /dev/mmc* "
brw-r----- 1 root disk 179, 0 Jan 1 00:00 /dev/mmcblk0
brw-r----- 1 root disk 179, 8 Jan 1 00:00 /dev/mmcblk0boot0
brw-r----- 1 root disk 179, 16 Jan 1 00:00 /dev/mmcblk0boot1
brw-r----- 1 root disk 179, 1 Jan 1 00:00 /dev/mmcblk0p1
brw-r----- 1 root disk 179, 2 Jan 1 00:00 /dev/mmcblk0p2
brw-r----- 1 root disk 179, 3 Jan 1 00:00 /dev/mmcblk0p3
brw-r----- 1 root disk 179, 4 Jan 1 00:00 /dev/mmcblk0p4
brw-r----- 1 root disk 179, 5 Jan 1 00:00 /dev/mmcblk0p5
brw-r----- 1 root disk 179, 6 Jan 1 00:00 /dev/mmcblk0p6
brw-r----- 1 root disk 179, 7 Jan 1 00:00 /dev/mmcblk0p7
brw-r----- 1 root disk 259, 0 Jan 1 00:00 /dev/mmcblk0p8
brw-r----- 1 root disk 259, 1 Jan 1 00:00 /dev/mmcblk0p9
UTP: sending Success to kernel for command $ ls -l /dev/mmc* .
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk0p1'
UTP: executing "dd if=$FILE of=/dev/mmcblk0p1"
8240+0 records in
8240+0 records out
4218880 bytes (4.0MB) copied, 1.659572 seconds, 2.4MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0p1.
utp_poll: pass returned.
UTP: received command 'frf'
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ newfs_msdos -F 32 -O android -c 8 /dev/mmcblk0p4'
UTP: executing "newfs_msdos -F 32 -O android -c 8 /dev/mmcblk0p4"
newfs_msdos: warning, /dev/mmcblk0p4 is not a character device
newfs_msdos: Skipping mount checks
/dev/mmcblk0p4: 25143232 sectors in 392863 FAT32 clusters (32768 bytes/cluster)
bps=512 spc=64 res=32 nft=2 mid=0xf0 spt=16 hds=4 hid=0 bsec=25149440 bspf=3070 rdcl=2 infs=1 bkbs=2
UTP: sending Success to kernel for command $ newfs_msdos -F 32 -O android -c 8 /dev/mmcblk0p4.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p5'
UTP: executing "mkfs.ext4 /dev/mmcblk0p5"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
131072 inodes, 524284 blocks
26214 blocks (5.00) reserved for the super user
First data block=1
Maximum filesystem blocks=67633152
64 block groups
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Superblock backups stored on blocks:
8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409

Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 36 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p5.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -O^extent /dev/mmcblk0p6'
UTP: executing "mkfs.ext4 -O^extent /dev/mmcblk0p6"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
65536 inodes, 262140 blocks
13107 blocks (5.00) reserved for the super user
First data block=1
Maximum filesystem blocks=67371008
32 block groups
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Superblock backups stored on blocks:
8193, 24577, 40961, 57345, 73729, 204801, 221185

Writing inode tables: done
Creating journal (4096 blocks): done
Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 38 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 -O^extent /dev/mmcblk0p6.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p7'
UTP: executing "mkfs.ext4 /dev/mmcblk0p7"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
131072 inodes, 524287 blocks
26214 blocks (5.00) reserved for the super user
First data block=0
Maximum filesystem blocks=536870912
16 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912

Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 20 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p7.
utp_poll: pass returned.
UTP: received command 'frf'
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p8'
UTP: executing "mkfs.ext4 /dev/mmcblk0p8"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
2048 inodes, 8188 blocks
409 blocks (5.00) reserved for the super user
First data block=1
Maximum filesystem blocks=8388608
1 block group
8192 blocks per group, 8192 fragments per group
2048 inodes per group

Writing inode tables: done
Creating journal (1024 blocks): done
Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 24 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p8.
utp_poll: pass returned.
UTP: received command 'pipe dd of=/dev/mmcblk0p5 bs=512'
pid is 3323, UTP: executing "dd of=/dev/mmcblk0p5 bs=512"
UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p5 bs=512.
UTP: received command 'frf'
573440+0 records in
573440+0 records out
293601280 bytes (280.0MB) copied, 35.521889 seconds, 7.9MB/s
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command 'pipe dd of=/dev/mmcblk0p2 bs=512'
pid is 3325, UTP: executing "dd of=/dev/mmcblk0p2 bs=512"
UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p2 bs=512.
UTP: received command 'frf'
9320+0 records in
9320+0 records out
4771840 bytes (4.6MB) copied, 1.081391 seconds, 4.2MB/s
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ echo Update Complete!'
UTP: executing "echo Update Complete!"
Update Complete!
UTP: sending Success to kernel for command $ echo Update Complete!.
utp_poll: pass returned.

Outcomes