AnsweredAssumed Answered

JB16 sample availability

Question asked by Oliver Scholz on Jun 30, 2008
Hello everyone,


I have noticed that the JB16DWE samples do not seem to be available anymore from Freescale, only the 20 pin package JB16JDWE is available. It seems that some pins used by the TBDML firmware are not bonded out on this package. Does anyone have attempted to adapt the firmware to work with the 20pin variant?

Or does anyone have a spare JB16DWE they'd be willing to slip into an envelope? I have a TBDML board here that I'd like to populate...

Maybe some kind soul responsible for Freescale's sample program recognizes the popularity of the TBDML project and makes this device available again?

Best regards,


Oliver

Outcomes