Hello,
After running bitbake fsl-image-minimal I'm getting the following error:
ERROR: OE-core's config sanity checker detected a potential misconfiguration.
Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).
Following is the list of potential problems / advisories:
The TMPDIR: /6113_sw/module/MY_CARD/linux/toolchain/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp can't be located on nfs.
Can you help ?
I do not need the folder to be NFS accessible.
Thank you,
Z.V
Check SDK installing sequence.
We usually use the following command sequence for SDK installing under Ubuntu 14.04 and Ubuntu 16.04:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
Have a great day,
Pavel Chubakov