Linux does not boot.
See the 'NoGoodCase_LinuxBoot.txt" please.
Is it related to CAAM (Cryptographic Acceleration and Assurance Module)?
platform caam_sm: [0016] ef 79 50 00 19 e2 5e 43 platform caam_sm: [0024] 68 35 44 35 82 29 1c 85 snvs-secvio 20cc000.caam-snvs: violation handlers armed - check state usbcore: registered new interface driver usbhid usbhid: USB HID core driver cs42xx8 1-0048: found device, revision 4 fsl-asrc 2034000.asrc: driver registered snd-soc-dummy snd-soc-dummy: ASoC: Failed to create platform debugfs directory imx-cs42888 sound-cs42888.25: cs42888 <-> 2024000.esai mapping ok imx-cs42888 sound-cs42888.25: snd-soc-dummy-dai <-> 2034000.asrc mapping ok imx-cs42888 sound-cs42888.25: cs42888 <-> 2024000.esai mapping ok imx-spdif sound-spdif.20: snd-soc-dummy-dai <-> 2004000.spdif mapping ok imx-audio-hdmi sound-hdmi.21: hdmi-hifi <-> hdmi_audio.3 mapping ok imx-tuner-si476x sound-fm.30: failed to find FM platform device imx-tuner-si476x: probe of sound-fm.30 failed with error -22 NET: Registered protocol family 26 TCP: cubic registered NET: Registered protocol family 10 sit: IPv6 over IPv4 tunneling driver NET: Registered protocol family 17 can: controller area network core (rev 20120528 abi 9) NET: Registered protocol family 29 can: raw protocol (rev 20120528) can: broadcast manager protocol (rev 20120528 t) can: netlink gateway (rev 20130117) max_hops=1 Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: BNEP socket layer initialized Bluetooth: HIDP (Human Interface Emulation) ver 1.2 Bluetooth: HIDP socket layer initialized 8021q: 802.1Q VLAN Support v1.8 Key type dns_resolver registered failed to disable 1.2 GHz OPP VGEN2: disabling VGEN2: couldn't disable: -5 SWBST: disabling SW4: disabling regulator-dummy: disabling imx mcc test is registered. usb_h1_vbus: 5000 mV usb_otg_vbus: 5000 mV ci_hdrc ci_hdrc.0: doesn't support gadget ci_hdrc ci_hdrc.0: EHCI Host Controller ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected UBI: attaching mtd3 to ubi0 random: nonblocking pool is initialized UBI: scanning is finished UBI: attached mtd3 (name "rootfs", size 8096 MiB) to ubi0 UBI: PEB size: 1048576 bytes (1024 KiB), LEB size: 1032192 bytes UBI: min./max. I/O unit sizes: 8192/8192, sub-page size 8192 UBI: VID header offset: 8192 (aligned 8192), data offset: 16384 UBI: good PEBs: 8086, bad PEBs: 10, corrupted PEBs: 0 UBI: user volume: 1, internal volumes: 1, max. volumes count: 128 UBI: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 1799680477 UBI: available PEBs: 0, total reserved PEBs: 8086, PEBs reserved for bad PEB handling: 150 UBI: background thread "ubi_bgt0d" started, PID 146 input: gpio-keys.18 as /devices/soc0/gpio-keys.18/input/input1 snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0) ALSA device list: #0: cs42888-audio #1: imx-spdif #2: imx-hdmi-soc UBIFS: recovery needed UBIFS: recovery deferred UBIFS: mounted UBI device 0, volume 0, name "rootfs", R/O mode UBIFS: LEB size: 1032192 bytes (1008 KiB), min./max. I/O unit sizes: 8192 bytes/8192 bytes UBIFS: FS size: 8177025024 bytes (7798 MiB, 7922 LEBs), journal size 33030144 bytes (31 MiB, 32 LEBs) UBIFS: reserved for root: 4952683 bytes (4836 KiB) UBIFS: media format: w4/r0 (latest is w4/r0), UUID 3511CB4F-9804-45B0-975E-3CDA9761602D, small LPT model VFS: Mounted root (ubifs filesystem) readonly on device 0:12. devtmpfs: mounted Freeing unused kernel memory: 328K (80d1f000 - 80d71000) INIT: version 2.88 booting Starting udev udev: Not using udev cache because of changes detected in the following files: udev: /proc/version /proc/cmdline /proc/devices udev: lib/udev/rules.d/* etc/udev/rules.d/* udev: The udev cache will be regenerated. To identify the detected changes, udev: compare the cached sysconf at /etc/udev/cache.data udev: against the current sysconf at /dev/shm/udev.cache udevd[176]: starting version 182 DBG sensor data is at 7f014218 ERROR: v4l2 capture: slave not found! UBIFS: completing deferred recovery UBIFS: background thread "ubifs_bgt0_0" started, PID 229 UBIFS: deferred recovery completed bootlogd: cannot allocate pseudo tty: No such file or directory Populating dev cache ALSA: Restoring mixer settings... No state is present for card cs42888audio Found hardware: "cs42888-audio" "" "" "" "" Hardware is initialized using a generic method No state is present for card cs42888audio No state is present for card imxspdif Found hardware: "imx-spdif" "" "" "" "" Hardware is initialized using a generic method No state is present for card imxspdif No state is present for card imxhdmisoc Found hardware: "imx-hdmi-soc" "" "" "" "" Hardware is initialized using a generic method No state is present for card imxhdmisoc Thu Jul 28 10:39:33 UTC 2016 <<===========last message line |
Original Attachment has been moved to: GoodCase_linuxBoot.txt.zip
Original Attachment has been moved to: NoGoodCase_LinuxBoot.txt.zip
what board used in the case - is it Sabre AI reference board ?
Please check that mfgtool2-yocto-mx-sabreauto*.vbs file was
used when programming with mfg tools
Hi yunbaekim
I do not think that caam is the reason, more probably this
is ddr errors or corrupted nand image. So make sense to change/rewrite
nand.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igorpadykov.
Always stop at same time( before print 'INIT: Entering runlevel: 5').
And same phenomenon appears when boot from SDCARD.
please try Demo Images from official i.MX6 product page
Hello igorpadykov~.
I tried Demo Images from official page('L4.1.15_2.0.0-ga_mfg-tools').
But the same result occurred.
See the log file please.
Header 1 |
---|
platform caam_sm: [0016] 9d f5 a1 ab 0a 2d ce bd platform caam_sm: [0024] 8f 20 2e ad fc 95 89 b8 snvs-secvio 20cc000.caam-snvs: can't get snvs clock snvs-secvio 20cc000.caam-snvs: violation handlers armed - check state usbcore: registered new interface driver usbhid usbhid: USB HID core driver cs42xx8 1-0048: found device, revision 4 fsl-asrc 2034000.asrc: driver registered imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok imx-cs42888 sound-cs42888: snd-soc-dummy-dai <-> 2034000.asrc mapping ok imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok imx-tuner-si476x sound-fm: failed to find FM platform device imx-tuner-si476x: probe of sound-fm failed with error -22 imx-audio-hdmi sound-hdmi: hdmi-hifi <-> soc:hdmi_audio@00120000 mapping ok NET: Registered protocol family 26 NET: Registered protocol family 10 sit: IPv6 over IPv4 tunneling driver NET: Registered protocol family 17 can: controller area network core (rev 20120528 abi 9) NET: Registered protocol family 29 can: raw protocol (rev 20120528) can: broadcast manager protocol (rev 20120528 t) can: netlink gateway (rev 20130117) max_hops=1 Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: BNEP socket layer initialized Bluetooth: HIDP (Human Interface Emulation) ver 1.2 Bluetooth: HIDP socket layer initialized 8021q: 802.1Q VLAN Support v1.8 Key type dns_resolver registered imx_epdc_fb 20f4000.epdc: can't get/select pinctrl ubi0: attaching mtd4 random: nonblocking pool is initialized ubi0: scanning is finished ubi0: attached mtd4 (name "rootfs", size 8096 MiB) ubi0: PEB size: 1048576 bytes (1024 KiB), LEB size: 1032192 bytes ubi0: min./max. I/O unit sizes: 8192/8192, sub-page size 8192 ubi0: VID header offset: 8192 (aligned 8192), data offset: 16384 ubi0: good PEBs: 8086, bad PEBs: 10, corrupted PEBs: 0 ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 ubi0: max/mean erase counter: 1/0, WL threshold: 4096, image sequence number: 1504641347 ubi0: available PEBs: 0, total reserved PEBs: 8086, PEBs reserved for bad PEB handling: 150 ubi0: background thread "ubi_bgt0d" started, PID 144 dhd_module_init in input: gpio-keys as /devices/soc0/gpio-keys/input/input1 snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0) VGEN2: disabling SW4: disabling ALSA device list: #0: cs42888-audio #1: imx-spdif #2: imx-hdmi-soc UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs", R/O mode UBIFS (ubi0:0): LEB size: 1032192 bytes (1008 KiB), min./max. I/O unit sizes: 8192 bytes/8192 bytes UBIFS (ubi0:0): FS size: 8177025024 bytes (7798 MiB, 7922 LEBs), journal size 33030144 bytes (31 MiB, 32 LEBs) UBIFS (ubi0:0): reserved for root: 4952683 bytes (4836 KiB) UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 9E8922F6-D319-4E3F-999D-062358AC85C8, small LPT model VFS: Mounted root (ubifs filesystem) readonly on device 0:14. devtmpfs: mounted Freeing unused kernel memory: 428K (80ae7000 - 80b52000) INIT: version 2.88 booting Starting udev udevd[174]: starting version 3.1.5 galcore: clk_get vg clock failed, disable vg! Galcore version 5.0.11.41671 ERROR: v4l2 capture: slave not found! UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 383 bootlogd: cannot allocate pseudo tty: No such file or directory Populating dev cache ALSA: Restoring mixer settings... No state is present for card imxspdif Found hardware: "imx-spdif" "" "" "" "" Hardware is initialized using a generic method No state is present for card imxspdif Fri Sep 16 20:32:27 UTC 2016 |