Hi,
I want to test TWR-K65f180m board with USB host and device. But in my folder Freescale_MQX_4_2 these examples are not available. Then I tried to clone for TWR-K65 but then also USB host and Device examples are not generated.
Is this the problem with my software or something.
If it is available with anyone please share.
Thanks and Regards,
Olivia
Hi Oliva:
This is a known issue in MQX 4.2 clone tool, USB stack and FFS are not generated in BSP cloning wizard for TWR-K65F180M board. Unfortunately we do not have a plan to fix this issue in the near future. You have to copy original project manually and rename it for use with cloned board. Sorry for the inconvenience that maybe caused.
Regards
Daniel
Hi Daniel,
Thank you for your reply. So it is not possible to clone for TWR-K65 board.
But can you share usb host and device stack for this board. Without that how can I work in MQX for this board.
our actual plan is to use K66. We are taking this as a reference .
Regards,
Olivia
Hi Olivia:
You can clone other parts for TWR-K65 board first, and manually copy usb later. The usb package is existed in MQX 4.2 install package.
There are two usb stacks in this MQX package
C:\Freescale\Freescale_MQX_4_2\usb
This one is an old usb stack, same as in MQX 4.1 and before
C:\Freescale\Freescale_MQX_4_2\usb_v2
This one is a new usb stack, same as the usb stack in KSDK, it is a complete new design.
Regards
Daniel