AnsweredAssumed Answered

what is the pinout for header connector on codewarrior tap

Question asked by Marty Smith on Nov 1, 2016
Latest reply on Nov 7, 2016 by Carlos_Mendoza

I am looking for the signal pinout of the codewarrior tap so that I can interface coldfire v2 core which is installed on a board developed by Arturus Networks which is not the standard 26 pin BDM interface. Arcturus has provided the 18 pin connector pin out for their board but I don't know the signals on the Codewarrior Tap module. If it matters I have the Rev E one.

Outcomes