AnsweredAssumed Answered

IMX6 use stagefright play MKV(avc+aac) video with error:MediaPlayer( 3316): Error (1,-1007)

Question asked by zero zero on Oct 31, 2016
Latest reply on Oct 31, 2016 by zero zero

Hi,

 

   The problem on the imx6q android4.2.2 and kernel 3.0.35.

   The same video can be played with omxplayer (not stagefright).

   The following is part of the log:

01-02 08:12:00.160 V/AwesomePlayer( 2238): MEDIA_ERROR -1007
01-02 08:12:00.160 V/MediaPlayerService( 2238): [3] notify (0x4221e6a8, 100, 1, -1007)
01-02 08:12:00.160 V/SurfaceTextureClient( 2610): SurfaceTextureClient::query
01-02 08:12:00.160 V/SimpleSoftOMXComponent( 2238): msgType = 2
01-02 08:12:00.160 V/AudioSystem( 3316): ioConfigChanged() event 0
01-02 08:12:00.160 V/AudioSink( 2238): stop
01-02 08:12:00.160 V/AudioTrack( 2238): stop 0x4221fe98
01-02 08:12:00.160 E/MediaPlayer( 3316): error (1, -1007)

 

 

Thanks.

Outcomes