Hi,
The problem on imx6 sabresd_6dq with android 4.2.2 and kernel 3.0.35.
Log print out a lot of the follow contents:
W/MediaPlayer( 3976): info/warning (3, 0)
E/OMXCodec( 2254): [OMX.Freescale.std.video_decoder.avc.v3.hw-based] dequeueBuffer failed w/ error 0xfffffff0
I/MediaPlayer( 3976): Info (3,0)
Thanks.
Actually, this is the effect of some memory segmentation issue of the 3.0.35 kernel. Migrating to later BSP with later kernel revision should fix the issue.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Can you kindly tell me which kernel version can be used on Android4.2.2? where to download? Can I only update kernel for my android system?
Thanks.
Q. Can I only update kernel for my android system?
A. No, it's not possible to only update the kernel. You have to completely migrate to later Android. Better to use the latest Marshmallow 6.0.1 BSP.