When testing the program eqadc cookbook simple scan does not read the input value that is connected to a potentiometer correctly. For example, when frame 5v brand eqadc 0x2380 in the result.
Attached circuit and CodeWarrior in the image.
Thank you.
Thanks
I would rather recommend to use codes from my examples shared here:
Example MPC5644A eQADC channel 146 conversion+calibration CW210
Example MPC5674F eQADC+eDMA Single_Scan CW210
Example MPC5674F eQADC+eDMA Continuous_Scan CW210
In the past I have tried it with MPC5634M as well - I am attaching example code.