AnsweredAssumed Answered

How to configure LS1046ARDB Linux for DHCP and DNS

Question asked by Sabine Schnabeltier on Oct 28, 2016
Latest reply on Aug 7, 2017 by Hunter Ware

Just setting up a LS1046ARDB to connect to internet. Board boots into Linux from flash drive to a filesystem extracted from fsl-image-full-ls1046ardb-20161022011454.rootfs.tar.gz. Have an internet router connected to RGMII1 port.

 

Added the following to the end of /etc/network/interfaces:

auto fm1-mac3
iface fm1-mac3 inet dhcp

 

After reboot, the board successfully obtains an IP address for the fm1-mac3 interface from the router.

 

Unfortunately, it does not configure the board's DNS automatically, even though it does save in /etc/resolvconf/run/interface/fm1-mac3 the nameserver it fetched from the router.

 

What else do I need to do to get DNS set up?

Outcomes