how to HM5065 work in imx6dl?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to HM5065 work in imx6dl?

714 Views
jianfeichang
Contributor IV

ov5640 is ok,now I have hm5065,Who has the driver code, I do not know how to start here

Labels (2)
0 Kudos
3 Replies

455 Views
ak_evident
Contributor I

Any success with HM5065? I receive D-PHY error when HM5065 is connected. Register 0x21dc014 value 0x00000330. Same settings for HM5065 work with Cypress CX3 bridge. Any idea?

Thanks, 

0 Kudos

626 Views
art
NXP Employee
NXP Employee

We don't have ready to use driver for the HM5065 camera. Use the source code of existing OV5640 driver to create the driver for HM5065.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

626 Views
joanxie
NXP TechSupport
NXP TechSupport

nxp don't have specific hm5065 driver, but one can refer to the porting document I attach, focus on Chapter 7
Supporting the i.MX 6Dual/6Quad/6Solo/6DualLite Camera Sensor with CSI, which tell you how to add new camera.

0 Kudos