Hi all,
I would like to use an IMX6 Dual Lite with less than 4 DDR3 chips, so in 16 or 32 bit DDR3 mode
Somebody can tell if this is possible ?
Thanks.
Hi Sébastien
yes this is possible
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for this answer.
Have you any datasheet or application note for bus use in 16 or 32 bit ?
I find documentation only for 1x64 bit (DDR3) or 2x32 bit (LP-DDR2).
Regards,
Sébastien
size is defined by MMDCx_MDCTL[DSIZ] DDR data bus size. Also one can check presentation on
DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations.pdf
Best regards
igor