i.MX7 NVCC_ENET1 power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 NVCC_ENET1 power supply

Jump to solution
579 Views
renofalkenberg
Contributor I

Hello,

Is it possible to use 2.5V for NVCC_ENET1?

I think there is a discrepancy between the datasheet (imx7dcec rev. 2) and the reference manual (imx7drm rev. 0.1).

The datasheet states only 1.8V and 3.3V as nominal supply voltages for NVCC_ENET1, while the reference manual states 1.8V, 2.5V and 3.3V (NVCC_ENET1 is outside of the state retention domain).

What is correct?

For my design it would make things much easier to use 2.5V.

Thanks and regards,

Reno

Labels (2)
0 Kudos
1 Solution
396 Views
igorpadykov
NXP Employee
NXP Employee

Hi Reno

you are right 2.5V also can be used.

Best regards
igor
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
397 Views
igorpadykov
NXP Employee
NXP Employee

Hi Reno

you are right 2.5V also can be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos