How to reset OCOTP_CFG5 and OCOTP_CFG6 using

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reset OCOTP_CFG5 and OCOTP_CFG6 using

613 Views
jackeyko
Contributor III

Dear NXP team,

I have wrriten OCOTP_CFG5 and OCOTP_CFG6 using fuse command in U-Boot.

 1) fuse prog 0 5  0x18000030

 2) fuse prog 0 6  0x00000010

I would like to reset OCOTP_CFG5 and OCOTP_CFG6 .

How to reset OCOTP_CFG5 and OCOTP_CFG6 using fuse command?

Thanks,

Jackey

Labels (1)
0 Kudos
2 Replies

457 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jackey

fuses are one time programmable and its state can not be reverted back.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

457 Views
jackeyko
Contributor III

Hi igor,

Thanks for your message.

Now, CPU Board(iWave i.MX6 Sodimm) is not working due to the changed OCOTP_CFG5 and OCOTP_CFG6.

iWave i.MX6 Sodimm is Download mode. How to aviod the download mode? 

iWave i.MX6 Sodimm Memory is using SPI NOR and eMMC.

SPI-NOR -> u-boot image

eMMC ->  Kernel Image and rootfs image

Thanks,

Jackey

0 Kudos