Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

684 Views
ryang
Contributor III

Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

Board name: MCIMX6Q-SDP

Andriod: M6.0.1_2.0.0

Subject: gpu rendering using adobe Air application APK and picture attached.

请先将runState.txt和floorInfo.txt放在 /sdcard/Parameter2里面,然后安装adobe air环境AdobeAIR.apk,再安装打开D1_1024_2.2.apk即可看到画面

Original Attachment has been moved to: D1_1024_2.2.apk.zip

Original Attachment has been moved to: AdobeAIR.apk.zip

Labels (1)
0 Kudos
2 Replies

547 Views
ryang
Contributor III

running=1&direction=2&currentFloor=25&currentMode=0&nextStopFloors=3,2,4&DFKR=0&scrollInterval=9

<root>
 <floor display="B1">
  <picURL>file://C:/Users/test/Parameter2/floorPics/b1.png</picURL>
 </floor>
 <floor display="1">
  <picURL>file://C:/Users/test/Parameter2/floorPics/1.png</picURL>
 </floor>
 <floor display="2">
  <picURL>file://C:/Users/test/Parameter2/floorPics/2.png</picURL>
 </floor>

</root>

0 Kudos

547 Views
igorpadykov
NXP Employee
NXP Employee

Hello rita

unfortunately I am not aware of Adobe Air use cases with i.MX6, for that

reason may be recommended to apply to MSS services for

help with integration Adobe freamework with i.MX6 Android.

Best regards
igor

0 Kudos