AnsweredAssumed Answered

QCVS (PA) Installation

Question asked by ralftruebenbach on Oct 25, 2016
Latest reply on Oct 27, 2016 by ralftruebenbach

Hello,

 

I'm trying to install the QorIQ Configuration and Validation Suite (for PowerPC T2080).

 

1) In QCVS_Install_Guide.pdf there is an all-in-one installer mentioned but at http://www.freescale.com/qcvs I can only find the offline installation packages for eclipse. Is the all-in-one installer still available?

 

2) I installed CodeWarrior for Power Architecture 10.5.1. But there is no "QorIQ Configuration Project" in File > New > (only CodeWarrior...ProjectWizard). Did I something wrong during the installation or do I have to install something else?
I also recognised that the "Available Software Sites" are quite empty (only 2 locations from eclipse.org). So I cannot update. Is there an update site for code warrior I can add?

 

3) I also tried to install the QCVS over my eclipse (online and offline) as described in "3.2 Installation over Eclipse" ending up with the error below. I think this is because my eclipse version 4.4 (Luna) is > 4.2?

 

An error occurred while installing the items
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --> [R]com.freescale.qcvs.feature_root 4.5.0.0001-20160210, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck).
org/eclipse/core/runtime/adaptor/LocationManager
org/eclipse/core/runtime/adaptor/LocationManager

Outcomes