Dear All,
Thanks for your help about the question!
ALSA device list:
#0: imx-spdif
RAMDISK: gzip image found at block 0
UDF-fs: warning (device ram0): udf_fill_super: No partition found (2)
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x65643030)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 1th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x642f0a30)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 2th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x65643030)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 1th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x642f0a30)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 2th superblock
UDF-fs: warning (device ram0): udf_fill_super: No partition found (2)
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x65643030)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 1th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x642f0a30)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 2th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x65643030)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 1th superblock
F2FS-fs (ram0): Magic Mismatch, valid(0xf2f52010) - read(0x642f0a30)
F2FS-fs (ram0): Can't find valid F2FS filesystem in 2th superblock
List of all partitions:
0100 8192 ram0 (driver?)
0101 8192 ram1 (driver?)
0102 8192 ram2 (driver?)
0103 8192 ram3 (driver?)
0104 8192 ram4 (driver?)
0105 8192 ram5 (driver?)
0106 8192 ram6 (driver?)
0107 8192 ram7 (driver?)
0108 8192 ram8 (driver?)
0109 8192 ram9 (driver?)
010a 8192 ram10 (driver?)
010b 8192 ram11 (driver?)
010c 8192 ram12 (driver?)
010d 8192 ram13 (driver?)
010e 8192 ram14 (driver?)
010f 8192 ram15 (driver?)
No filesystem could mount root, tried: ext3 ext2 ext4 vfat msdos iso9660 ntfs fuseblk udf f2fs
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
I do it:
android-info.txt imx6sl-evk-csi.dtb recovery.img
boot.img installed-files.txt recovery-imx6sl.img
boot-imx6sl.img kernel root
clean_steps.mk obj symbols
dex_bootjars previous_build_config.mk system
fake_packages ramdisk.img system.img
fsl-sdcard-partition-f2fs.sh ramdisk-recovery.img system_raw.img
fsl-sdcard-partition.sh recovery u-boot.imx
gen recovery.id u-boot-imx6sl.imx
Hello Joshua,
I’m sorry to hear you’re having problems running android on the i.MX6SL. I’m assuming you’re using the i.MX6SEVK as denoted by your device tree.
You may use the Manufacturing Tool to create and load the Android filesystem. Please make sure to use the manufacturing tool that matches the Android version you are using. You may find them on the following link under programmers:
The other alternative is using the SD card partition script, which creates the necessary partitions after which you may load each with the required files. There is detailed information on how to do this on the “Storage partitions” section of the Android User's Guide.
It would be something like:
$ cd ~/myandroid/
$ sudo chmod +x ./device/fsl/common/tools/fsl-sdcard-partition.sh
$ sudo ./device/fsl/common/tools/fsl-sdcard-partition.sh -f <soc_name> /dev/sdX
# <soc_name> can be imx6q, imx6dl, imx6sl, imx6sx and imx7d.
I hope this helps!
Regards,