AnsweredAssumed Answered

Error launching FRDM-K64F_MQXL_FLASH_OpenSDA ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device

Question asked by Michael Smorto on Oct 23, 2016
Latest reply on Nov 3, 2016 by ZhangJennie

I am trying to compile and flash the NXP sensor funsion rev 5 and trying to following the instructions using a K64f freedom board with codewarrior 10.7 (latest one just downloaded for windows 7.  I am using the opensda and receiving the following error when I do a run configuration:

 

Error launching FRDM-k64F_MQLX_FLASH_OpenSDA ARM GDI Protocol Adapter.  Cannot connect . The Debugger can not connect to the P&E Device.

 

I have no idea what I am doing as this is my first experience with MBED - coming from a Arduino background.  So keep it simple

 

 

THanks

Mike

Outcomes