Hi,
I've built yocto BSP with the following configuration.
DSTRO=fsl-imx-x11 MACHINE=imx6qsabreauto source fsl-setup-release.sh -b bld-x11
bitbake fsl-image-gui
It generated .sdcard and I could boot i.MX with this image file.
However, I cannot find basic development tools such as "make" and "gcc" in the distro.
How can I have those development tools?
Hi Bio_TICFSL,
Thank you for your answer. I got gcc and make commands.
Here are what I did.
bitbake fsl-image-gui # I need to run this to create local.conf first.
echo "EXTRA_IMAGE_FEATURES += \"dev-pkgs tools-sdk\"" >> conf/local.conf
cd ../
DISTRO='fsl-imx-x11'
MACHINE='imx6qsabreauto'
source ./setup-environment bld-x11
bitbake -ccleanall fsl-image-gui
bitbak fsl-image-gui
Though this flow works, it seems redundant as I need to compile once and then re-compile all again.
Can you think of any smarter way to do this?
Regards,
Masa