Hello,
Can the iMX6 BOOT_CFG pins (that need to be Low OR the ones that says "Reserved" in the Fuse Table) connected straight to Ground (instead of pulling to gnd using resistors). This will save me pcb space by getting rid of components
Thanks
Chirag
Hi Chirag
recommended to follow standard practice for connection techniques
on the PCB during system development, please check sect.3.3.3 i.MX Connection
Leakage due to Unstable State During Power-Up AN2537 Power Network Design
http://cache.freescale.com/files/32bit/doc/app_note/AN2537.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igore, can you pls also answer this question that I’ve posted to the one you already replied? (see attached)
Hi Igor,
For clarification purpose, does SD4 port on iMX6 Quad also support emmc 4.41? The reference manual indicates only SD3 port supports 4.41 (see attached snapshot from ref manual).
What's mode does SD4 support? DDR, SDR?
Thanks
Chirag